Other Parts Discussed in Thread: AWR1642
Hi,
I have downloaded the industrial toolbox version 3_6_2 and tried to use the people counting lab. the console is empty and I have done everything right.
Steps I followed:
1. Flash the .bin file from the people counting folder
2. switch off the mm-wave radar and remove the SOP2 jumper and then turn it on again
3. Give permission to these two ports /dev/ttyACM0, and /dev/ttyACM0 before opening the mmwave visualizer
4. select the mmwave SDK version
5. send config to mmwave device and I am able to connect both ports
6. Press the NRST switch(SW2). after that, it shows " Hardware connected'
7. Again press the send config to mmwave device.
8. But the console is empty.
Where did I make wrong? if someone has any idea. kindly please post in the comments.
Do I need to place the AWR1642 mmwave radar at a height of around 1-1.5 meters to make it work?
Thanks