This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA302: Datasheet clarification

Part Number: PGA302

     Hello,

I work with pga302 datasheet and have a couple of questions:

        Q1.  In the datasheet internal voltage reference TC  specified  as +/- 250 ppm/C.

                Is this typo ? 

        Q2.  My project is - design pressure transmitter. The sensor is piezoresistive bridge. 

                Assume , the sensor is ideal .  What could be the best accuracy , that  pga302  can achieve ?

                On page 68, table 67  the numbers  look strange. E.g. VINPP - VINPN = 34.651 mV,  VOUT EXPECTED  =  0.5 V

                                                                                                       VINPP - VINPN  = 13.844 mV,    VOUT EXPECTED  =  2.5 V 

                                                                                                                  ---- 

                 I assume that gain is the same for all rows. Please, explain.

    Thank you in advance,

Ruben