Other Parts Discussed in Thread: AWR1642,
Hi,
About profile change dynamically, in SDK rl_sensor.h and interface control guide, it describes it is able to change profile dynamically without RF stop. But per my previous test on AWR1642 and some discussion on E2E, seems it is unfeasible, need to modify with RF stopped firstly. Here would like to get your confirmation, look forward to your reply soon, thanks.
@note 2: This API can be issued dynamically to change profile parameters.
* Few parameters which cannot be changed are
* 1. numAdcSamples
* 2. digOutSampleRate
* 3. Programmable filter coefficients in AWR2243/xWR6243/AWR29xx
* 4. The dynamic profile configuration settings are applied to HW at the end of the 
* active frame boundary (start of the frame idle time). It is recommended to issue 
* dynamic profile config API at the beginning of the active frame (during the 
* chirping) to apply the profile changes for immediate next frame
BR,
Andy