Other Parts Discussed in Thread: LDC1000EVM, LDC1101, LDC3114
Hello,
My customer plans to use LDC1041 for their new design.
They designed an L using WeBench, it is supposed to around 1.2uH.
The L is on their target PCB with a C, 1500pF, in parallel.
They connected their target PCW to LDC1000EVM as follows.
They tried to tune the Filter capacitor on the LDC1000EVM so that CFB pin waveform amplitude gets around 1Vpp.
But, they were not able to see significant amplitude at the CFB pin with 20pF to 1000pF filter capacitor range.
What does TI think is wrong?
Does TI think any suggestions to solve the issue about the L and the C on their target PCB, the Filter capacitor on the LDC1000EVM or any register settings?
What setting is recommended for amplitude bits in the LDC Configuration register?
Best regards,
K.Hirano