Other Parts Discussed in Thread: IWR6843ISK
Hi, I have a MWAVEBOOST. 2x IWR6843ISK-ODS and one and IWR6843ISK module.
After successfully debugging both IWR6843ISK-ODS modules, I encounter a sudden error this morning while starting a debug session:
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.8.0.00235)
Testing the ccxml file function, it seems that there is an error in the USCIF driver:
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
Reading through https://software-dl.ti.com/ccs/esd/documents/ccs_debugging_jtag_connectivity_issues.html#invalid-data-read-back did not solve the problem. Both IWR6843ISK-ODS show the same error. The IWR6843ISK is working, but the code is not showing any output in the console while running the overhead_3d_people_count_68xx_mss project.
What could be wrong here?