Other Parts Discussed in Thread: AWR1843
Hi There,
I am trying to do the beam steering using the AWR1843BOOST board and need all three antennas to be ON. I wonder if it is sufficient to set the transmit antenna mask to 7 in channelCfg command. The command used in script is:
channelCfg 15 7 0
and then I did change in chirpCfg command:
chirpCfg 0 0 0 0 0 0 0 7
Is it sufficient to turn ON all three transmitter antennas?
Am I doing it correctly and how can I confirm the same? Could you please provide any information on it? Many Thanks.
Anu