Other Parts Discussed in Thread: AWR1843BOOST, , AWR1843
In the associated previous thread the following details were given
-------------------------------------------------------------------------------
The AWR1843AOP has an angular accuracy which is not as good as the AWR1843BOOST EVM with PCB antennae.
For angles < +/- 45 deg, we measured 5deg angle accuracy. For larger angles, 10+ degrees.
Angular accuracy can be improved using multi angle calibration.
------------------------------------------------------------------------------------------
whether accuracy of +/- 1 degree can be achieved.
If so how to do,
Please clarify,
Thank you