Part Number: IWR6843AOP
I am trying to integrate and deconflict several radars using the "Hardware Trigger" and "Frame Trigger Delay in ms" mentioned in the SDK user guide. My goal is to trigger the system at 40Hz. I have verified that my configuration is good and I am getting the expected 40Hz RX rate when my frame trigger delay is set to 0.0ms. However, once I increase the frame trigger delay to a value greater than 1.0ms the frame rate I receive over UART drops from 40Hz to 20-30Hz. Is this expected?