Hi,
We are using MMCAS-RF-EVM(1243) and MMCAS-DSP-EVM for sampling ADC data. According to our test, the maximum sampling rate is 18.75MHz and maximum adcSampleNum is 512.
In that case, the maximum range and range resolution can not meet our requirements.
Is it possible that we can improve this parameters? Our expecting maximum range is 200m and expecting range resolution is 0.05m.