Dear Team,
Do we have solution can replace SHTC3, The working temperature is between 60-70.
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Thanks for posting to the Sensing forum!
We have a wide range of humidity sensors in our portfolio that are highly accurate between a temperature range of -40°C to 125°C. The latest family of devices, HDC3X have a better supply range and a better accuracy. However, none of these sensors are P2P compatible with the SHTC3.
Regards,
Pavani Tenneti