Part Number: OPT3006
Other Parts Discussed in Thread: OPT3007
Dear Expert
Opt3006, the IIC address is set as 1000100 according to the specification. It has been in large quantities before, and the IC works normally (check the surface mark of the IC that works normally recently, and the text on the IC is "6F 7").
This inspection found that the IC could not be driven and could not work normally (the text on the IC is "6F 2").
Since OPT3007 is also in use at the same time, we tried to use the IIC address "1000101 "of OPT3007 to drive "OPT3006 for this exception", and found that OPT3006 worked
Therefore, it is inferred that there is something wrong with the incoming material of OPT3006.