Hi,
I want to use the MSS_UARTB_RX and I coding below.
---------------------------------------------------------------------
---------------------------------------------------------------------
---------------------------------------------------------------------
Pinmux_Set_OverrideCtrl(SOC_XWR16XX_PINP4_PADBB, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);
Pinmux_Set_FuncSel(SOC_XWR16XX_PINP4_PADBB, SOC_XWR16XX_PINP4_PADBB_MSS_UARTB_RX);
/* Setup the default UART Parameters */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.clockFrequency = MSS_SYS_VCLK;
uartParams.baudRate = 115200;
uartParams.isPinMuxDone = 1U;
/* Open the Logging UART Instance: */
gSrrMSSMCB.loggingUartHandle = UART_open(1, &uartParams);
if (gSrrMSSMCB.loggingUartHandle == NULL)
{
System_printf("Error: MMWDemoMSS Unable to open the Logging UART Instance\n");
return;
}
#define BUF_SIZE (512)
char buf[BUF_SIZE] = {0};
if (UART_readPolling(gSrrMSSMCB.loggingUartHandle, (uint8_t *)buf, sizeof(buf)))
{
UART_writePolling(gSrrMSSMCB.loggingUartHandle, (uint8_t *)buf, strlen(buf));
}
else
{}
---------------------------------------------------------------------
---------------------------------------------------------------------
---------------------------------------------------------------------
It don't work and I don't know how to slove it.
Can you support with me?
Thanks