I have a problem with AWR164 boost in the idea that after I flash it with the interferer .bin file from interference mitigation project C:\ti\mmwave_platform_1_2_1\labs\interference_mitigation\interferer, this is not transmitting any signal. I observed that after I flash the bin, and remove the SOP 2, jumper, the device does not appear in Device Manager/Ports and also I observed that the led DS1 is blinking continuously.
I mention that if I flash it with the bin file that corresponds to the victim radar the sensor is working fine.