Hello everyone
I am working on an application in which I want to use TMAG5273 sensor. In this application, I need to sense harmonic magnetic field ripples (amplitudes are around 200uTpeak, sinusoidal at 100Hz) in the presence of a constant background magnetic field (ranging from -20mT to 20mT).
I am basically wondering how much the measurement of the small, sinusoidal magnetic field ripple amplitude will change as a function of applied background magnetic field.
The datasheet mentions the "sensitivity linearity error" for the A1 characteristic as 0.1%. So does this mean, that if I slowly change the constant background magnetic field from -20mT to 20mT, the measurement of the AC magnetic field amplitude should only change by approx. 0.1%?