Hi,
We are trying to obtain height of a vehicle approacihng or departing ramp on public parking. Detection and counting of cars is fine, only we get confusing results with measuring height of the object. Sensor is at approx. 3m height with 5 degrees tilt toward the ground. The scenary parameters are pasted below.
staticBoundaryBox -12 12 5 14 0 3
boundaryBox -10 10 6 12 0 3
gatingParam 6 5 10 5 10
stateParam 20 20 60 40 10 100
allocationParam 60 80 0.1 6 40 5
maxAcceleration 1 2 1
trackingCfg 1 2 200 10 135 422 100
sensorPosition 3 0 5
presenceBoundaryBox -10 10 6 12 0 3
The strange values for Z coordinate we obtain from TLV7 as the mean value of the Z coordinate through the frames the specific target appears in the scene. Often we obtain the negative values for the Z coordinate, X and Y coordinate are OK. Can you explain me in detail how the sensor calcuates the Z coordinate and please share with me scene geometry in this specific case. We use the modified chirp configuration file from the D:\mmwave_industrial_toolbox_4_11_0\labs\Traffic_Monitoring_chirp_configs\18xx_traffic_monitoring_70m_MIMO_3D.cfg.
Please, we need to solve this issue as urgent as possible because we have customer presentation in 3 days.
Thanks in advance, Veljko