Other Parts Discussed in Thread: AWR1843BOOST, MMWAVEICBOOST
Hello Champs,
HW: AWR1843AOPEVM
SW: C:\ti\mmwave_automotive_toolbox_3_6_0\labs\lab0016_automated_parking
mmwave SDK 3.6 or mmwave SDK 3.5
CCS v12.0
Customer did following tests.
(1) xwr18xx_mmw_aop_demo.bin + GUI is OK
(2) mmwave_sdk_03_06_00_00 or mmwave_sdk_03_05_00_04 xwr18xx_ccsdebug.bin + \prebuilt_binaries\aop\xwr18xx_mmw_aop_demo_dss.xe674 and xwr18xx_mmw_aop_demo_mss.xer4f is OK
But CCS prompted exit.c error message when opening GUI.
[Cortex_R4_0] **********************************************
Debug: Launching the MMW Demo on MSS
**********************************************
Debug: Launched the Initialization Task
Debug: mmWave Control Initialization was successful
Debug: mmWave Control Synchronization was successful
[C674X_0] Debug: DPM Module Sync is done
[Cortex_R4_0] Debug: CLI is operational
Debug: Sending rlRfSetLdoBypassConfig with 3 1 0
Error: DPM Report 4 received with error:-40112 arg0:0x64 arg1:0x8003e88
{module#9}: "../mss_main.c", line 2174: error {id:0x10000, args:[0x1891c, 0x1891c]}
xdc.runtime.Error.raise: terminating execution
[C674X_0] Error: DPM Report 4 received with error:-40112 arg0:0x64 arg1:0x815c9c
xdc.runtime.Main: "../dss_main.c", line 256: assertion failure
xdc.runtime.Error.raise: terminating execution
Is it a bug for the lab0016_automated_parking demo?
Thanks
Rgds
Shine