Hi,
Our customer uses a disk-shaped magnet that is divided into 8 parts by N/S in order to detect the speed/angle of the motor.
Two Hall ICs are placed at the position with a phase difference of 90°.
Is the orientation of the Hall IC important when two sensors are placed on the same circumference with a certain angular interval between them?
For example, below, are A) and B) the same sensitivity?
Best regards,
Hiroshi