Hello E2E Experts,
Good day.
I can't make it work in sleep and wake mode to give me an interrupt when the sensor makes a new measure. Attached I send the sensor's configuration just before I write the DEVICE_CONFIG2 with the value of 0x13. Have in mind that I read the configuration from the sensor.
One more. When I give the command for Wake up and sleep (DEVICE_CONFIG_2 = 0x03) the device first sleeps or first measures? If first measures then there is no point to use this mode in order to save power.
Workflow
1. Put the sensor into Wake up and sleep
2. Device measure and exit mode since INT_CONFIG_1 = 0xA4
3. Read angle value
3 Put the sensor again in Wake up and sleep mode
This leads to a continuous mode.
Correct me if I am wrong
Thank you in advance for your support.
Regards,
CSC