Hi,
I am trying to my sensor to work with 1Tx/4Rx configuration. There are antenna configurations like 1Tx/1Rx, 1Tx/2Rx or 1Tx/4Rx for other sensors. But there are no configs for awr1843aop, it is limited to 2Tx and 3Tx configurations in OoB visualizer.
I tried to do it myself with .cfg which is below and I can't get an azimuth data output at this time.
sensorStop flushCfg dfeDataOutputMode 3 channelCfg 15 3 0 adcCfg 2 1 adcbufCfg -1 0 1 1 1 lowPower 0 0 % 3D short range profileCfg 0 77 2 4.1 36.72 0 0 15.79 1 208 6578 0 0 30 % 2D long range profileCfg 0 76 2 3.8 12.35 0 0 9.85 1 93 12311 0 0 30 % chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 2 % chirpCfg 2 2 1 0 0 0 0 1 % advFrameCfg 2 0 0 1 0 subFrameCfg 0 0 0 2 48 100 0 1 1 100 subFrameCfg 1 0 2 1 32 100 0 1 1 100 % guiMonitor 0 1 0 0 0 0 0 guiMonitor 1 1 0 0 0 0 0 % cfarCfg 0 0 2 8 4 3 0 10 0 cfarCfg 0 1 0 4 2 3 1 12 0 % cfarCfg 1 0 2 8 4 3 0 10 0 cfarCfg 1 1 0 4 2 3 1 12 0 % multiObjBeamForming 0 1 0.5 multiObjBeamForming 1 1 0.6 % calibDcRangeSig 0 0 -5 8 256 calibDcRangeSig 1 0 -5 8 256 % aoaFovCfg -1 -90 90 -90 90 cfarFovCfg 0 0 0.25 20 cfarFovCfg 1 0 20 150 cfarFovCfg 0 1 -30 30 cfarFovCfg 1 1 -30 30 % CQRxSatMonitor 0 3 15 125 0 CQSigImgMonitor 0 115 6 CQRxSatMonitor 1 3 15 125 0 CQSigImgMonitor 1 115 6 % analogMonitor 0 0 lvdsStreamCfg -1 0 0 0 clutterRemoval -1 1 bpmCfg -1 0 0 0 % compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 measureRangeBiasAndRxChanPhase 0 1. 0.2 extendedMaxVelocity -1 1 %
Thank you.