Other Parts Discussed in Thread: , MMWAVEICBOOST
Hi!
I'm currently working on developing a product that is using the IWR6843 device. The custom pcb we have designed is identical to the IWR6843ISK REV A except for the antenna part. We have added a horn antenna. The firmware running on the device is based on the lab 19 from the industrial toolbox 3.2.0 and SDK 3.1.1.2. We want to use the libraries from the "Low Power Demo" but they are only compatible with the SDK-version 3.5.x.x.
What I want to know if those libs can be ported to our firmware will sticking to a old toolbox and SDK or if you suggest using a new newer versions? I have also seen that some labs are only supported for IWR6843ISK REV B or higher. Is this the case for the newer toolboxes and SDK's?
Best regards / Christoffer