Hi,
What's the max sample rate of IWR1843. It states "The maximum ADC sampling frequency in the TI’s radar devices is 37.5 MHz (AWR1xxx)". However, when I set the digOutSampleRate to 15000 in the configuration file, the program terminates with error "Error: mmWave Start failed [mmWave Error: -3101 Subsys: 0] {module#9}: "../mss_main.c", line 3219: error {id:0x10000, args:[0x1a0bc, 0x1a0bc]}".
Thanks.