This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: SPI clock levels between host board and BOOST eval board

Part Number: AWR2243


G'day everyone,

We're trying to interface with the AWR2243 chip and program it over SPI, but are having many troubles. Currently, we're using a host board with output lines connected to the BOOST eval board for testing.

When we try SPI write from the host board, the clock signal (yellow) varies between 0-3 V:

Photo of analyser when only connected to host. SPI clock signal (yellow) goes between 0-3 V.

When the BOOST board is connected the clock signal now goes between 1-2 V:

Photo of analyser when connected to host and BOOST board. SPI clock signal (yellow) goes between 1-2 V.

As you can see, the clock signal changes level between the two photos. This could disrupt the interpretation of high and low states. Any assistance in debugging this issue would be much appreciated!

Cheers,

Jacob