I want to accurately measure the temperature of a surface with the LMT87. To this end, it would be important to place the correct side of the sensor on the surface. The datasheet states: "To ensure good thermal conductivity, the backside of the LMT87 die is directly attached to the GND pin". I would want to place this "backside" on the surface. However, I am a bit confused about which side this is. Would the backside be the side of the sensor that has the smaller surface area due to the taper or the other side?
Any help is much appreciated