This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Support for dynamically changing chirp frequencies

Part Number: AWR1843

Hello,

I'd like to ask about methods of changing the chirp frequency during runtime.

I understand that the AWR1843 provides one such method of cycling through different chirp set parameters using multiple mmWave BSS profiles (max 4, MMWAVE_MAX_PROFILE). However, is there a mode separate from the profiles on the AWR1843 such that the device will cycle through a given set of frequencies?

For instance:

1. Define chirp frequencies (a, b, c, d)
2. Start device. Enable 'frequency_cycling' mode. Supply 'frequency_cycling' config with frequencies in (1).
3. Device automatically switches through frequencies in (1).

Thanks,

Norman