This IWR6843ISK EVM is a new one which i just ordered from TI.com on Feb.22 2023. And I test it on Mar. 1st
After set the SOP as attateched image, I install the CP210x_Windows_Drivers( download from https://www.silabs.com/documents/public/software/CP210x_Windows_Drivers.zip)
and I also try the https://www.silabs.com/documents/public/software/CP210x_Windows_Drivers.zip, my system is window10 X64) .
Then I connect the IWR6843ISK to my PC with USB cable, then I find the LED status is abnormal, Just D6 is green, D3,D4 and D5 are off-status,
and the same time, I cannot find the simulated 2 COM ports on the Device Manager of my PC.
1、 I am sure the USB cable is good, because I can use it to connect other devices.
2、 I tried different PCs,the problem exist also.
How can I solve this problem? The LED status is abnormal means the EVM has something wrong?