Greetings,
I am currently using the LDC1614EVM in conjunction with 36mH coils. To achieve a resonance frequency of 1.1kHz, I attempted to use a 560nF capacitor. Unfortunately, the resonance frequency readings are proving to be unstable, and the correct value for the coil is not being measured. My suspicion is that this may be due to the proximity of the cutoff frequency of 1kHz. I have tested this hypothesis using capacitors of 470nF and 330nF, but the same behavior persists.
I would greatly appreciate any recommendations or advice you may have regarding this issue.
Thank you kindly in advance.