Other Parts Discussed in Thread: AWR1843
I follow the DCA1000EVM CLI Software User Guide to collect the raw data from the DCA1000 with an AWR 1843BOOST in Windows. Everything is Ok and I collect the raw data successfully, but the data is just incorrect. See the range-doppler map I got as below, only one target is moving but there are 4 targets showing in the range-doppler image.
After that, I use the mmwave studio to repeat the experiment and collect the raw data. Then I generate another range-doppler map as below, you can see there is only one target shown as expected.
So there are two differences between these two cases:
1) DCA1000EVM CLI Software vs mmwave studio
2) 18xx_demo.bin from the mmWave_Demo_Visualizer vs xwr18xx_radarss.bin & xwr18xx_masterss.bin from mmwave studio
Could someone help me to see what's wrong with this?
Best,
Kevalen