This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: high_accuracy_14xx_mss project CCS debug

Part Number: IWR1443BOOST

Hi team,

Here's an issue from the customer may need your help:

1) The customer wants to debug the high_accuracy_14xx_MSS project using CCS. Flashed debug.bin and ran the project as shown in Figure 1 of the manual. However, in Figure 2, Load Config from PC and Send is not responding, the GUI window has no feedback so cannot know if the profile has been sent. Is the program not working properly? 

Figure 1

Figure 2

2) The DFT mode of Hwa is used in the Zoom FFT operation of this project. The customer would like to know is there any docs specify on how the algorithm configures parameters in this mode? Especially the values in red checkmarks (they have referenced Radar Hardware Accelerator and Radar Hardware Accelerator-Part 2) .

Could you help look into this case? Thanks.

Best Regards,

Cherry

  • 1) The customer wants to debug the high_accuracy_14xx_MSS project using CCS. Flashed debug.bin and ran the project as shown in Figure 1 of the manual. However, in Figure 2, Load Config from PC and Send is not responding, the GUI window has no feedback so cannot know if the profile has been sent. Is the program not working properly? 

    Can you ask the customer to try this with Tera Term or a similar serial tool? They should see output on the secondary uart line at 921600 baud if so.

    2) The DFT mode of Hwa is used in the Zoom FFT operation of this project. The customer would like to know is there any docs specify on how the algorithm configures parameters in this mode? Especially the values in red checkmarks (they have referenced Radar Hardware Accelerator and Radar Hardware Accelerator-Part 2) .

    The document that the customer is using specifies these parameters. We don't have any specific docs that discuss the way this lab is set up.

    Best,

    Nate