This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP75: Temp. register reading

Part Number: TMP75

HI,

   TMP75 uses 2 bytes of temperature register. but if customer reads Byte 1 only, what will be happened? Is it possible to happen as below case?

In some specific applications, when only the MSByte is read using a single-byte read command, it often happens that if bit D7 of the LSByte is zero, then the device will hold in a LOW state forever, resulting in a bus hang-up problem, and the bus cannot be released until the device power is reset.