This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Issues related to hardware version, firmware version, etc. in device information

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

The following figure shows the device information of the development board iwr1443 chip obtained during debugging.

1.Does hwMajor and hWMinor represent the device as ES3.0, or does the version information of ES3.0 correspond to one of the following parameters?

2.Does fwMajor and fwMinor represent the firmware version of the device as 2.0, or does the firmware version correspond to one of the following parameters?

3.Is there a document that explains the specific meaning of the following parameters?

4.Do you have any help documents on how to identify device hardware version, firmware version, and supported SDK features?