Other Parts Discussed in Thread: FDC1004
Hello, I'm trying to use the FDC2114 for a research project and am able to measure various capacitances.
I'm a little puzzled since most of the data sheet images are drawn as single ended configurations (with sensor connected one way to GND)

However this is not the way I can measure appropiate values of capacitors. This only works in differential setup where Cmeas is between InA and InB.
Also this is the only succesfull way I'm able to apply the mentioned formula, which also refers to differential configuration.


Question A: what are the settings to use this chip in single ended configuration and which formula can be used to measure?
For research we try to measure and understand the resonant circuit driver in differential mode.
The image I get on the scope when measuring between GND and A on channel 1 and GND and B on channel 2 looks like this:

Question B: I would have expected a complete sinusoidal signal, can someone explain how this circuit measuring exactly.
Hope someone can explain the questions.