Other Parts Discussed in Thread: UNIFLASH, , IWR6843, MMWAVEICBOOST
Hello Team,
Posting on behalf of my customer:
I am trying to program an IWR6843AOP on a custom board using the SPIA interface connected to an FT2232 chipset. I am using the Uniflash Tool to flash the out of the box demo and it detects the XDS100v2 USB Debug
Probe (which is actually not connected) and two COM Ports provided by the FTDI chip.
When trying to flash the out of the box demo, I get an error message:
error: Initial response from the device was not received. Please power cycle device before re-flashing.
error: Not able to connect to serial port. Recheck COM port selected and/or permissions.
I would like to clarify following points:
1. Is it necessary to flash an image over QSPI using a FT4222H or does the SPIA interface in combination with the FT2232 work as well? According to the App Note "IWR6843 Bootloader Flow" for a similar chipset, this should be possible (section 2.2).
2. Is an external Flash memory (e.g. MX25R1635FZUIH0) necessary in both cases (SPI and QSPI)?
3.Is it necessary to set the SOP pins first in flashing mode and then in functional mode to flash an image over SPIA? According to the document "IWR6843 Bootloader Flow" (Figure 4), this should be possible in functional mode as well.
Regards,
Renan