This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA305: INP+, INP- is not used, also floating OK? and ADC sampling rate

Expert 3040 points
Part Number: PGA305


Please let me know if pin of INP+/- are not used, floating is OK?

In addtion to above, customer want to konw spec of ADC sampling rate, what's the parameter of output rate and response tme? 

Best Regards, ny 

  • Hi NY,

    Please let me know if pin of INP+/- are not used, floating is OK?

    Yes, it is okay to leave them floating.

    In addtion to above, customer want to konw spec of ADC sampling rate, what's the parameter of output rate and response tme? 

    Output rate:

    Data rate of the ADC is ~7.8kHz or 128us. Usually this is in the electrical characteristics section but it seems like it isn't listed there. For example you can find that answer in the overview section:

    And in plenty of other sections as well. 

    Response time:

    There's another one here:

    Best,

    -Cole