Part Number: TMCS1108-Q1

Hello,
I am using TMCS1108A1U-Q1 IC to measure voltage as well as current in channel. According to my Design I have connected Current IC output to my 16-Bit Resolution ADC Channel. So, I have main issue with my current ic is when my load is connected and consuming some of voltage nearly 2.8V those i have measure with my DMM but when i place check this voltage in IC output i just got only 0.28V this is not a actual voltage after getting this voltage i used some of equation mention in a Datasheet and calculate current i got -1 A.
Calculation:
Vout = 0.28 V
S = 50 mV/A
Vout,oa = Vin * 0.1
Vout,oa = 3.3 * 0.1 = 0.33
So,
Vout = S x I(in) + Vout,oa
0.28 V = (50mV/A) * I(in) + 0.33 V
I(in) = (0.28 - 0.33) / (50mV/A)
I(in) = - ( 0.05)*(1000) / 50
I(in) = -1A
I have used as this equation for current calculation.
CASE 2:
Once i disconnect my all load and measure voltage on current IC i can get 0.33 V this is correct voltage i get as per datasheet because there are have one equation to calculate voltage in 0A
Here, Input Voltage is 3.3 V
so,
Vout,oa = 0.1 * Vs
Vout,oa = 0.1 * 3.3 = 0.33
Also i have mad one calculation using datasheet value and checked maximum voltage what i am getting i have used for that,
I(in) = 54.5 A
S = 50 mV/A
Vout,oa = 0.33 V
So,
Vout = S * I(in) + Vout,oa
Vout = (50 mV/A)*(54.5A) + (0.33 V)
Vout = 3.1 V
Here also i have checked i can't get maximum Vout as 3.3 V but i have given 3.3 to so i am assuming i need maximum voltage get as 3.3 V in Vout also.
Ideally i am assuming that when i connect my load i need to get some current in positive as well as match voltage with the DMM and calculation formula in so i am requesting you to please provide any formula for linear current calculation, also I have attached schematic for your reference.
Thanks & Regards,
Fenil
NOTE: I have application on Linear Reading based so i am taking input and all parameter accordingly.