Other Parts Discussed in Thread: IWR6843, , AWR6843
Hi team,
Regarding the SWRU520E doc of TRM and SWRA627 doc of IWR6843 Bootloader Flow, the customer has the following questions:
1) According to the system interconnect diagram on page 256 of 520e document and the IWR6843 Interconnect diagram in page 2 of RA627 document:
Is there only one way to connect the PCR-2 bridge with respect to the two bus crossbar modules, SCR_64bit and PCR_32bit? That is, the DMA is connected to the PCR separately. This allows the core to access one of the interface modules on the PCR.
For example, when configuring the UART, the DMA can simultaneously transfer to the register space of other interface modules. When the DMA is configuring the address space of other interfaces (I2C) on the Core, it can transfer data to Mibspi's SRAM simultaneously, enabling drivers for both IPs on the code side at the same time? If so, does the DMA need to introduce a cable from the DMA to the lower interconnect in the RA627 documentation?
2) On page 32 of SPRUIV5B document for AWR294x:
The master on SCRP indicates that there are two masters of R5F and two masters from SCRM, as well as the main ports of the DSS and BSS subsystems. Will there be a conflict accessing which slave port of the interface PCR module? Or can the interface SPIA/B be accessed individually by multiple subsystems at the same time? But the SCRP to MSS PCR in the figure above draws only one line.
Could you help check this case? Thanks.
Best Regards,
Cherry