Part Number: LM63LM64LM96X63EVM
Other Parts Discussed in Thread: LM63, , LM96194, LM94, LM96000, LM93
Do you have a new version of the LM63 evaluation board that is now compatible with windows 10?
Thank,
Aslam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sorry, there is no updated software for LM63LM64LM96X63EVM.
ren
not software, updated hardware or a new item/ similar item that can control PWM of at least 2 devices simultaneously.
The LM96000, LM93, LM94 and LM96194 all have at least 2 PWM channels. None of these legacy devices have an EVM.
thanks,
ren
Ren,
I need a PWM controller that i can plug a DC fan into and control through a GUI on my PC and is compatible with windows 10..... it should be able to control at least two fans independently and simultaneously. I do not need temperature readings or anything else. i just need 4 pins, gnd, pwr, tach, and pwm that is pluggable (meaning no soldering required like the EVM).. I do not need an a IPD or the LM-line of components. There are a lot of devices available on the market that can do this, i wanted to know what TI's latest product in this category is. If it does not have one, then I will look elsewhere. Please advise. Thanks
Okay. It was a good product, wish TI continued support/ updates.
Thanks for your time, Ren. Appreciate the support.