This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP513: Configuration of TMP513

Part Number: TMP513

Hello Team,

We use the TMP513 to get temperature data, the local temp is right, but remove temp is error with negateive data, do you have any configuration application note or reference for us.

Thanks!

Temp=39.3 -191.4 -192.5 -190.7
Temp=39.4 -191.3 -192.5 -190.7
Temp=39.6 -191.3 -192.5 -190.6
Temp=39.6 -191.3 -192.5 -190.5
Temp=39.8 -191.2 -192.5 -190.5
Temp=39.9 -191.2 -192.5 -190.4
Temp=40.0 -191.2 -192.5 -190.4
Temp=40.1 -191.0 -192.4 -190.5
Temp=40.3 -191.0 -192.5 -190.3
Temp=40.4 -190.9 -192.4 -190.3
Temp=40.5 -190.9 -192.5 -190.3
Temp=40.6 -191.0 -192.3 -190.3
Temp=40.7 -190.8 -192.3 -190.2
Temp=40.8 -190.8 -192.4 -190.3
Temp=40.9 -190.8 -192.3 -190.2
Temp=41.1 -190.7 -192.4 -190.1
Temp=41.3 -190.7 -192.3 -190.0
Temp=41.4 -190.5 -192.3 -190.0
Temp=41.5 -190.5 -192.3 -190.0
Temp=41.7 -190.3 -192.3 -190.0
Temp=41.8 -190.3 -192.3 -190.0
Temp=41.9 -190.3 -192.3 -189.9
Temp=42.1 -190.3 -192.3 -190.0
Temp=42.3 -190.2 -192.3 -189.9
Temp=42.4 -190.1 -192.2 -189.7
Temp=42.6 -190.0 -192.2 -189.7
Temp=42.8 -190.0 -192.2 -189.8
Temp=42.9 -190.0 -192.1 -189.7
Temp=43.0 -189.8 -192.2 -189.7
Temp=43.1 -189.8 -192.3 -189.7
Temp=43.4 -189.8 -192.2 -189.7
Temp=43.5 -189.8 -192.2 -189.6
Temp=43.6 -189.6 -192.2 -189.5
Temp=43.8 -189.6 -192.2 -189.5
Temp=44.0 -189.6 -192.0 -189.5
Temp=44.1 -189.5 -192.0 -189.4
Temp=44.3 -189.5 -192.2 -189.5
Temp=44.4 -189.5 -192.0 -189.4
Temp=44.6 -189.3 -192.1 -189.3
Temp=44.7 -189.2 -192.0 -189.2
Temp=44.9 -189.2 -192.1 -189.3
Temp=45.0 -189.2 -192.0 -189.3
Temp=45.1 -189.2 -192.0 -189.2
Temp=45.3 -189.0 -192.0 -189.2
Temp=45.5 -189.2 -192.0 -189.0
Temp=45.6 -189.0 -192.0 -189.0
Temp=45.8 -189.0 -192.0 -189.0
Temp=45.8 -189.0 -192.0 -189.0
Temp=46.0 -189.0 -191.9 -189.0
Temp=46.1 -188.8 -192.0 -189.0
Temp=46.3 -188.9 -192.0 -188.9
Temp=46.4 -188.8 -191.8 -188.9
Temp=46.6 -188.8 -191.8 -188.9
Temp=46.7 -188.8 -191.8 -188.8
Temp=46.8 -188.7 -191.8 -188.8
Temp=47.0 -188.8 -191.8 -188.7
Temp=47.1 -188.6 -191.8 -188.7
Temp=47.3 -188.6 -191.8 -188.7
Temp=47.4 -188.6 -191.8 -188.7
Temp=47.6 -188.6 -191.8 -188.7
Temp=47.6 -188.5 -191.7 -188.6
Temp=47.8 -188.4 -191.8 -188.6
Temp=47.9 -188.4 -191.8 -188.5
Temp=48.1 -188.3 -191.7 -188.6
Temp=48.1 -188.3 -191.8 -188.5
Temp=48.3 -188.3 -191.6 -188.5
Temp=48.4 -188.3 -191.8 -188.3
Temp=48.6 -188.3 -191.7 -188.5
Temp=48.6 -188.2 -191.6 -188.4
Temp=48.8 -188.2 -191.6 -188.4
Temp=48.9 -188.1 -191.6 -188.3
Temp=48.9 -188.1 -191.6 -188.3
Temp=49.1 -188.2 -191.7 -186.8
Temp=50.1 -188.0 -191.5 -178.5
Temp=50.8 -187.9 -191.4 -171.5
Temp=51.5 -187.7 -191.5 -172.5
Temp=52.4 -187.6 -191.3 -173.5
Temp=52.9 -187.4 -191.3 -174.2
Temp=53.6 -187.3 -191.3 -174.5
Temp=54.3 -187.3 -191.3 -175.8
Temp=55.4 -187.3 -191.2 -172.3
Temp=56.1 -187.3 -191.3 -166.4
Temp=56.7 -187.4 -191.3 -164.0
Temp=57.5 -187.4 -191.2 -162.6
Temp=58.8 -187.3 -191.3 -162.6
Temp=59.9 -187.2 -191.2 -163.2
Temp=61.1 -187.2 -191.3 -164.2
Temp=62.8 -187.0 -191.2 -164.5
Temp=63.9 -187.0 -191.2 -164.5
Temp=65.0 -186.9 -191.2 -164.3
Temp=66.1 -186.8 -191.2 -164.2
Temp=67.6 -186.8 -191.2 -164.5
Temp=68.7 -186.7 -191.0 -164.8
Temp=69.6 -186.6 -191.0 -163.3
Temp=70.4 -186.7 -191.0 -161.3
Temp=70.9 -186.5 -191.0 -160.8
Temp=71.4 -186.5 -191.0 -160.7
Temp=71.8 -18&.3 -190.9 -160.3
Temp=72.9 -186.3 -190.9 -160.2
Temp=73.6 -186.2 -190.9 -159.9
Temp=74.2 -186.2 -190.9 -159.8
Temp=74.9 -186.2 -191.0 -163.2
Temp=75.6 -186.1 -191.0 -166.1
Temp=76.1 -186.0 -190.9 -168.0
Temp=76.6 -185.9 -190.9 -169.3
Temp=77.1 -185.9 -190.8 -170.4
Temp=77.6 -185.8 -190.8 -171.0
Temp=77.9 -185.8 -190.8 -171.5