This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: What is the minimum distance AWR1843 can detected using lab demo mrr?

Expert 2050 points
Part Number: AWR1843

Can you please advise what is the minimum distance AWR1843 can detected using lab demo mrr?

I tested AWR1843 by puting my hand in front of the AWR1843Boost, when the distance reduces to ~4cm, it seems the device could not detect the object.

Kind regards  

  • Hi Lei,

    Please make sure that the distance to measure is greater than the range resolution of the device (4.3cm in this case for USRR). Less than 4cm is too small a gap between the sensor and the object for it to be able to resolve it. The range config can be found in the chirp definition.

    Regards,

    Kaushik