This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5011: compatible with TMR1202S

Part Number: DRV5011
Other Parts Discussed in Thread: TMAG5123

Is there p2p compatible with TMR1202S with push-pull output? thanks. 

+/-17Gauss

RB

Brian

  • Brian,

    One challenge to add to this is that the referenced device is sensitive to the field which is in the X direction due to having been built with TMR.  To truly be P2P with this device, our device would need to be sensitive to the field in this direction as well.  Currently, we only offer TMAG5123 with this sensitivity direction in a SOT23-3 package.

    This device samples at 10 kHz, but the highest sensitivity option (TMAG5123B) has a typical threshold at 4.1 mT (41 G).  The temperature range matches, but operating supply current on this device is 3.5 mA, which is due to the difference in sample rate and sensor type (Hall vs. TMR). The other drawback is that the output type on this sensor is open-drain.

    If the direction of sensitivity can be flexible, then TMAG5231C1G has a typical threshold at 3 mT, push-pull outputs, and samples at 216 Hz.  The average current for this device is 16 uA.

    Thanks,

    Scott

  • Thanks for feedback. it looks it doesn't work due to the power consumption, BW. and others parameters...etc. application is an Encoder with multi-turn. the power consumption is also important. 

    Does TI have TMR sensor plan in the future?

    Regards

    Brian

    Regards

    Brian

  • Brian,

    I will send you a direct message to discuss future devices.

    Thanks,

    Scott