This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: SYNC_IN signal monitor / Diagnostics

Part Number: AWR1843

Hi,

My customer uses multiple AWR1843 devices in the system and each device is synchronized with SYNC_IN signal so that multiple radar transmissions are not overlapped.
Under such environment, if SYNC_IN signal is lost (stopped), it seems the system is completely stopped.

The customer wants to monitor SYNC_IN signal and if something wrong happens (the signal stops, noises are applied, etc.),
they want to stop the system safely and restart it.
What is the recommended way to realize above usecase in the device?

Thanks and regards,
Koichiro Tashiro