- Does the TI Thermistor Design Tool allow the use of lower order polynomials?
- Does the TI Thermistor Design Tool provide expected min and max temperature error for the condition of using “nominal fixed values for polynomials”, Rbias resistor tolerance of either 1% or 0.5%, and no overall Gain and Offset final calibration (this would be done at final Functional Test if needed to be added)? We see min/max in the resistance tables but not sure if they are being utilized.
Thank you!