I want to verify the position of a 12Vdc 1amp solenoid valve. Would it be possible to use a LDC to monitor the inductance change of the solenoids coil as the armature moves through it? Based off the response in the related post this is possible but the LDC needs to be isolated from the power going through the coil. How would this be done? Where do the high impedance inductors need to be placed? Is there a referance design? Regarding referance designs I did review the TIDA-00289 design where the back emf of the coil is used to determine the position, unfortanitly this will not work with this vavle due to very little back emf (no measurable current cusp). A screen capture showing the voltage (yellow) and current (blue) when the valve is actuated is attacheched.