This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP75: Register 0xF

Part Number: TMP75
Other Parts Discussed in Thread: TMP1075

Hello,

I performed a register read for register 0xF (which is not mentioned in the datasheet) and found that it contains the value 7500. This is the same value that the TMP1075 datasheet specifies would be in that register on the TMP1075. Why am I able to get that value from register 0xF on the TMP75? Does the register exist but it is reserved on the TMP75? Are there any issues with reading from that register when using the TMP75?

Thank you!

Best regards,

Zach Kimble