Other Parts Discussed in Thread: IWR6843
Hello,
I am testing the AWR6843AOPEVM hardware with Windows 10.
I flashed the hardware with "out_of_box_6843_aop.bin".
Then, I used mmWave_Demo_Visualizer, SDK version 3.6 to visualize how the hardware works. It works.
I flashed the hardware with "vital_signs_tracking_6843AOP_demo.bin".
Same, I used mmWave_Demo_Visualizer, SDK version 3.6.
I connect the serial ports the same way.
In the messages console, nothing is displayed.
At the bottom left, by clicking on the small triangle I have the following two messages:
CLI_CFG_port connected (COM14:115200)
DEMO_OUTPUT_DAT_port - connecting (COM15:921600, waiting for data ...)
Should I use a specific application for "vital_signs_tracking_6843AOP_demo.bin"?
Thank you for your help.
Regards.