This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP1827EVM: ask for a API or COM library

Part Number: TMP1827EVM

for a fast test setup we would like to use the EVM board with connected sensor in a laboratory test setup.

Is there a description of the COM protocoll available which is used by the EVM software? I would like to read the temperature values from EVM board by serial interface with an own software application and would like to prevent the effort to assemble a µC board if it is on the table with this EVM. All I found were the code samples for a host application.