Hello,
We're using the TMP302 in an application and getting varying accuracy results.
- Looking for some layout suggestions.
- Which pin on the IC is used for temperature measurements?
- Not able to connect up any pins on the IC to the high temperature copper pour.
Current layout (below)
:
Proposed updated layout (below)
Pour copper under IC and use VIAs to connect pins to internal layers
Pull away copper on layers 2, 3, and 4 under the IC
Thank you for your help, Keith