Other Parts Discussed in Thread: TMP1827
When changing the EVM by breaking out the TMP1827 board and switching to bus powered configuration, the EVM is reading all 0xFF's. Is there a special configuration to be made so the GUI can switch from VDD to VPUR?
I am assuming the pullup resistor needs to be changed according to the equation 2 of the datasheet. If using 3.3V as Vdd, the resistor range should be between 750Ω and 2.2kΩ. We should then replace R9, currently at 390Ω.
Thank you!