The LUT table in the datasheet is for a Vdd of 2.7V, but as I will use either a 3.3V or 5.0V supply for these sensors, can TI provide LUT tables for these two voltages?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LUT table in the datasheet is for a Vdd of 2.7V, but as I will use either a 3.3V or 5.0V supply for these sensors, can TI provide LUT tables for these two voltages?
Hi Richard,
The LUT table shown in the LMT70 datasheet applies to the entire supply voltage range since the output voltage is not supply dependant. The snapshot below shows the supply-induced error (PSR).
Best regards,
Simon Rojas
Hi Simon,
Thanks for the reply and confirming that the supply is independent of the TAO output.
For the supply induced error, if I were to use a 3.3V supply for all my temp sensors, how do I compute the error for the LUT readings?
Regards,
Richard.
Hi Richard,
Usually you could treat PSR as a linear equation. However, this device has a characterization over different temperature/supply ranges. In this case, I would recommend using the min/max limit for error budget calculations. This would include 9 mC/V from -55 C to 120 C and 15 mC/V from 120 C to 150 C.
With that you could account for a max error of around 30 mC from -55 C to 120 C and 50 mC from 120 C to 150 C.
Best regards,
Simon Rojas