Other Parts Discussed in Thread: LDC2112, FDC1004, LDC2114
Greetings,
We are in the process of integrating a custom coil design based on the LDC2112 sensor IC. We have recently purchased a LDC2114EVM development board along with reference coil designs. The reference coils seem to work out of the box with the default configurations of the Sensing Solutions EVM GUI tool, but using a custom coil seems to give no results. The custom coil (referenced in the image below) has the following parameters: Flex PCB, thickness 0.11mm, coil dimensions 8x16mm (racetrack), trace width 6mil, space between traces 5mil, 2 layers, 11 turns, 0.333 oz. copper. Could someone please guide me through the parameter configuration of the sensor IC (and possible HW changes i.e. changing the Ccom capacitor value on the LDC2114EVM) so that we can get some usable and detectable results from the coil?
Thank you very much,
Yours sincerely,
Stefan