Hi,
I'm developing a position detection system to control the position of a shaft as it slides past the hall sensor (see my picture below).
Due to space constraints, the magnet is fitted to the shaft.
The air gap between the magnet and the sensor is 1mm at the moment, although i can probably increase it if necessary.
The shaft has to be made from hardened steel, which is of course magnetic! Please could someone advise what effect will this have on the ability of the DRV5056-Q1 to sense the position of the magnet?
Thanks in advance.
Andrew